{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the equivalences for the capacitive opening retarders, part numbers LA9Z, for DC coil contactors?
NOTE: This accessory is obsolete without replacement. This FAQ is to provide legacy information only. Note also that the Tesys F range (LC1F references) is also obsolete. See Tesys GIGA range for replacement contactors.

The equivalences for the capacitive opening retarders in the old LC1F range and the new LC1F range are as follows:
Old part number New part number
LA9Z90F LAZR90F
LA9Z90MLAZR90M
LA9Z90QLAZR90Q
LA9Z91FLAZR91F
LA9Z91MLAZR91M
LA9Z91QLAZR91Q

This accessory is no longer available in the Tesys D range.

For information, attached to this documentation are:

An extract of the 1995 catalogue detailing the LA9Zxxx part numbers for LC1D and LC1F contactors
An extract of the current catalogue detailing the LAZR9xxx part numbers

Schneider Electric Ireland

Attachment(s)
PCP2_167.pdf [31.96 KB]
Section B9 page 16 2019 Motor Control & Protection.pdf [175.72 KB]
PCP2_166.pdf [45.87 KB]