Welcome to the Schneider Electric Website

You can visit our website in another country or region or go to our global website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais

Uniflair Monoblock Room Cooling

Wall mounted units for indoor installation for mission critical applications

Rapidly deployable packaged systems to quickly address cooling needs of IT or telecom environments

Uniflair Monoblock Room Cooling
  • Features

    The Uniflair MB is a wall mounted cooling unit installed on the outside of a conditioned space, such as a telecom enclosure. These units are completely self-contained, meaning they are shipped completely charged and there is no need for a remote heat exchanger. These rapidly deployable units only require simple electrical wiring and mounting to the shelter. Available in a free cooling configuration, these units come equipped with motorized dampers to enable use of the outside air to help cool the IT space

    Benefits

    Availability
    • Dual power inputs - (Optional) Dual power supplies for incoming power redundancy
    • Redundant Components - Single points of failure in the system have redundant components to maintain availability and reliability.
    • Direct drive motors - Stress on bearings is nearly eliminated, increasing useful life. Allows integral fan/motor assembly to be factory balanced, which lowers vibration and expedites startup.
    • Active response control - Monitors and actively adjusts cooling capacity to ensure proper server inlet temperatures. Through the microprocessor controller, visibility into the operation and status of the unit is provided.
    • Scroll compressors - Utilize few moving parts for increased reliability and life expectancy.
    Manageability
    • Network interface - Provides management by connecting the device directly to the network with a dedicated IP address, avoiding the need for a proxy such as a server. Management is available via Web browser, Telnet or SSH. Notification features inform you of problems as they occur.
    • Building Management Systems - Units are designed to work with the most common BMS systems including BACnet and Modbus.
    • Local area network - Creates a shared control between all the available resources for maximum energy efficiency and controlled management of the group during emergency situations
    • Microprocessor controller - Provides proactive control and real-time monitoring via a four line, eighty character, alphanumeric display.
    Serviceability
    • Service monitoring - All the monitoring devices on board the unit allow for preventive maintenance and a check of the working condition of the system while its in operation.
    • Easy service access - Allows for all serviceable components to be replaced/maintained by easily accessible panels/doors.
    • Operational Service - Allows critical components to be maintained/replaced while the system is in operation.
    Total cost of Ownership
    • Direct Free Cooling - Utilizes outdoor air when ambient air temperature can help support cooling loads.
    • High performance technological solutions - Optimize the unit operation at any load or ambient condition, guaranteeing an extremely low power consumption
    • Modular strategy - Modular design of the mechanical and control systems allow for gradual build-up of the cooling infrastructure to match the cooling demand of the facility. This greatly reduces CAPEX expediture and provides deferred investment throughout the life of the facility.

EcoStruxure™ for Your Business

EcoStruxure lets you thrive in today's digital world. Make better business decisions with scalable and converged IT/OT solutions.

Reach Us

Have a question, complaint or is there some feedback you’d like to send us to make your experience with Schneider Electric better?