המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where can a NetShelter CX be deployed?
Issue:
Where can the NetShelter CX be deployed?

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Need to make sure that the NetShelter CX will function properly in the environment into which it is being installed.

Resolution:

•Large office with air-con - Best conditions. All sizes of NetShelter CX with maximum thermal load will work comfortably.
•Small office with air-con - Good conditions. All sizes of NetShelter CX with maximum thermal load will work comfortably.
•Large office, no air-con - Good conditions. All sizes of NetShelter CX with maximum thermal load will work comfortably.
•Small offices with no air conditioning - Larger sizes of NetShelter CX with maximum thermal load will potentially require additional cooling assistance from an open window or portable air conditioning device. For loads of more than 2kW we recommend you contact APC by Schneider Electric, Technical Support.
•Note: All of these scenarios assume that CX load and positioning guidelines are followed.
•Guidelines can be found in the Unpack & Install guide available on the CX product pages of the APC website.