{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

באפשרותך לבקר באתר שלנו במדינה אחרת או באזור אחר או לעבור לאתר האינטרנט הגלובלי שלנו.

בחר את המיקום שלך

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}
Search FAQs

How do I know which is the parameter value is currently displayed on a DM6000 and PM1000 Series meter?

Press any one of the 5 keys once; meter will display the parameter name of the current page under display.
Or
If none of the keys are pressed and if the auto scroll is also not enabled, then the meter repeatedly displays the current page parameter name (2sec) and value (8sec).
Or
If the auto scroll is enabled, then the meter will display the current parameter name (1sec) and value (4sec) and moves to the next page. Refer quick start guide for more details on auto scroll


Legacy KB System (APS) Data: RESL200934 V1.0, Originally authored by DaMi on 01/07/2010, Last Edited by DaMi on 01/07/2010
Related ranges: PM1000 series, DM6000 series
Explore more
Explore more

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.