המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
EM64XX THD issue in Meter display and through communication.
EM64XX THD issue

Goals and Symptoms

Summary
EM64XX THD issue in Meter display and through communication.

Symptoms
The EM64XX power meter shows current THD% as ----in the meter display and -999 through communications.

Causes and Fixes

Cause
1. When the secondary current is less than and equal to 10% or greater than and
equal to 110% of CT ratio.
2. When frequency is greater than 65Hz.

Resolution
In order to get the THD reading proper we need to maintain

1. Secondary current should be greater than 10 % and should be less than 110% of CT ratio.
2. Frequency should be less then 65 Hz.

All the necessary information is available in User Manual and QSG.


שניידר אלקטריק ישראל

קבצים מצורפים
Final - Digitan.7z [22.57 MB]