המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why does PowerChute Network Shutdown not start after upgrading system Java?
Issue:
After upgrading system Java PowerChute Network Shutdown web interface is not accessible.

Product:
PowerChute Network Shutdown versions v3.x, v4.0, v4.1, v4.2

Environment:
All supported OS

Cause:
When upgrading Java in most cases the older version in uninstalled so the path PowerChute uses to access Java no longer exist.

Solution:
Run the PowerChute installer which will discover the new path.

NOTE: This issue is resolved in PowerChute Network Shutdown v4.3+ which supports OpenJDK.