שאלות נפוצות
Osisense XC - Tightening torque values of the XCMD mounting screws, not delivered with the limit switch
For the XCMD blue limit switches, such as for the XCSM red safety switches, the recommended tightening torque of the 2 mounting screws in the casing, are the following; provided for a maximum screw diameter of 4 mm (millimeter) or 0.157 in (inch) :
- minimum torque value : 1 N.m (Newton x meter) or 8.85 lb.in (pound x inch)
- maximum torque value : 1.5 N.m or 13.27 lb.in
Attached XCSM instruction sheet extract providing these values
- minimum torque value : 1 N.m (Newton x meter) or 8.85 lb.in (pound x inch)
- maximum torque value : 1.5 N.m or 13.27 lb.in
Attached XCSM instruction sheet extract providing these values
פורסם עבור:שניידר אלקטריק ישראל
קבצים מצורפים
גלה עוד