שאלות נפוצות
What are the part numbers for the flange mounting kits for the Altivar Process drives?
Issue:
Altivar Process drives flange mounting kits.
Product Line:
Altivar Process Drives (ATV630, ATV930)
Environment:
Altivar Process Drives
Cause:
Part number required to order part
Resolution:
Mounting bracket for flange-mounting kit for NSYPTDS1, NSYPTDS2, NSYPTDS3 is NSYAEFPFPTD. This is a stand off bracket, optional to push the enclosure away from the wall.
Instruction Sheets attached
Altivar Process drives flange mounting kits.
Product Line:
Altivar Process Drives (ATV630, ATV930)
Environment:
Altivar Process Drives
Cause:
Part number required to order part
Resolution:
Mounting bracket for flange-mounting kit for NSYPTDS1, NSYPTDS2, NSYPTDS3 is NSYAEFPFPTD. This is a stand off bracket, optional to push the enclosure away from the wall.
Instruction Sheets attached
פורסם עבור:שניידר אלקטריק ישראל
קבצים מצורפים
גלה עוד
גלה עוד