המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
In the NetShelter WX 6U Vertical cabinet, must the included 2U UPS Mounting Bracket be used?
Issue:
It's unclear if the included 2U UPS Mounting Bracket must be used.

Product Line:
AR106V, AR106VI

Environment:
All versions and serial ranges.

Cause:
The AR106V/VI ships with a 2U UPS Mounting Bracket.

Resolution:

If the UPS is being installed into the cabinet prior to shipping, the 2U Mounting Bracket is required.
If the cabinet is not shipping with the UPS installed, then the UPS may be installed with its own mounting brackets.