undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the probable causes & remedy of SCF (Motor Short Circuit) fault in Altivar 312 drive.
Probable Cause:
  • Short-circuit or grounding at the drive output
  • Significant ground leakage current at the drive output if several motors are connected in parallel
Remedy:
  • Check the cables connecting the drive to the motor and the motor insulation.
  • Reduce the switching frequency
  • Connect chokes in series with the motor

Schneider Electric India

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: