Browse FAQs

Is it possible to read single phase meters as well as three phase meters modbus registers at the same time from BCPM

Published date: 13 September 2018

Yes, there should be no problem to read the SINGLE-PHASE METERS MODBUS POINTMAP as well as 3-PHASE METERS MODBUS POINT MAP at the same time.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.