{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Does Quantum safety PLC support modbus port address swaping during hotstandby switchover.
For Quantum Safety 140CPU67160S PLC the %SW60.8 control is unavailable, hence it is not possible to have modbus port switching functionlity .
Basically the system word %SW 60 is used for hot standby control functions and the bit 8 of the word %SW60 is used to control the behaviour of
Modbus port in normal 67160 Quantum PLCs.
If %SW60.8 =0 address switches on Modbus port 1 during a primary swap. If %SW60.8=1 no address switches on Modbus port 1 during a primary swap.

Schneider Electric India