undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to terminate “Move Velocity” configured as Data set type in Motion Sequence operating mode for Lexium 32M range of servo drive.
While operating Lexium 32M range of servo drive in “Motion Sequence” operating mode, data set type configured as “Move Velocity” can be terminated
only if parameter of respective data set “Transition type” is set to “Abort and Go Next”. Aborting of “Move velocity” will be done as per settings of
parameter “Transition Condition 1”, “Transition Value 1”, “Transition Condition 2” and “Transition Value 2”. Following abortion of “Move Velocity” Data Set
will be followed as per setting of parameter “Subsequent Data Set”.

Schneider Electric India

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: