On the ATV71 torque limitation, are the Motoring torque limit (tLIM) and Gen. torque limit (tLIG) values based on the torque rating of the motor or on the ratings of the drive?
Published date:
06 August 2019
Issue:
What is the torque rating based on? On the ATV71 series, Motoring torque limit (tLIM) and General torque limit (tLIG) state that they can be adjusted between 0 and 300% of the rated torque.
Product Line:
ATV71
Environment:
All model and serial numbers
Cause:
None
Resolution:
The nominal torque is calculated in the drive on the basis of the motor parameters entered into the drive.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.