undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to read registers for circuits 43-84 from a Branch Circuit Power Meter (BCPM or BCPMSC).
The BCPM register list only contains register addresses for circuits 1-42. To read circuits 43-84 you will need to read the same registers for circuits 1-42 on the next modbus address. For instance if the BCPM is configured to modbus address 1, you will read circuits 1-42 exactly as the register list details. For circuits 43-84 you will read the same registers using modbus address 2. This principle also applied when adding an 84 circuit BCPM to an EGX or ECC card, you will need to add the configured address and the proceeding address.

Schneider Electric India

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: