Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
What are the valid address range settings for the Advantys STBNDN2212 DeviceNet Network Interface Module (NIM)?
Issue
DeviceNet Address
Product Line
Advantys STB
Resolution
As a single node on a DeviceNet network the Advantys STBNDN2212 NIM requires a unique network address with respect to other nodes on the network. The valid address range settings are from 0 to 63.
Did this answer your question?
Explore more
Range:
Explore more
Range: