Browse FAQs

Can the same mechanical interlock for LC1FL44 contactor be used for mechanical interlock of the new equivalent LC1F6304 contactor.

Published date: 13 September 2018

Yes, the same mechanical interlock LA9FL970 can be used for both the old LC1FL44 as well as for new equivalent LC1F6304 contactors. This is a horizontally mounted mechanical interlock.
 
For the new LC1F6304 contactor a vertically mounted mechanical interlock LA9FL4L is also available.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.