Browse FAQs

Is it possible to use the universal encoder card VW3A3409 with Altivar 71 drive.

Published date: 29 July 2019

Yes, it is possible to use the universal encoder card VW3A3409 but you have to use an ATV71 S383 drive for the recognition of universal encoder. 
Refer to attached file. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.