Browse FAQs

What is the difference between "RotMonOn" and "ShowEncPos" in Lexium SD328 drives.

Published date: 13 May 2019

For Lexium SD328 stepper drives range,

When CTRLS_MotEnc = "ShowEncPos" is meant to have motor encoder connected. Stepper drive will show the position of motor encoder. But Rotation Monitoring will remain De-activated. This means "Flt_pDiff" ( Difference between Reference position and Actual position) will not be monitored. Fault A320 - tracking error too high is not detected

When CTRLS_MotEnc = "RotMonOn" is meant to have motor encoder connected. Stepper drive will show the position of motor encoder. Rotation monitoring will be activated. This means "Flt_pDiff" ( Difference between Reference position and Actual position) will be monitored. Fault A320 - tracking error will be detected.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.