Browse FAQs

What are the logical functions are available in VAMP 255/245/230 relay's also state maximum output & input gates available.

Published date: 15 May 2019

The device supports customer-defined programmable logic for boolean signals. The logic is designed by using the VAMPSET setting tool and downloaded to the device. 

Functions available are:
1. AND
2. OR
3. XOR
4. NOT
5. COUNTERs
6. RS & D flip-flops
Maximum number of outputs is 20. Maximum number of input gates is 31. An input gate can include any number of inputs.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.