How can you disable the mode button on the face of the ATV312 drive so you can not put the drive in local mode?
Published date:
09 August 2019
Issue:
How can you disable the mode button on the face of the ATV312 drive so you can not put the drive in local mode?
Product Line:
Altivar ATV312
Environment:
All
Cause:
Needs to disable the Local button so that no one can put the drive in local mode my mistake.
Resolution:
You can not disable the Mode button all together. If you set a password in Pin 1 the mod button will then only switch between SUP menu and frequency reference.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.