Browse FAQs

What will be the maximum permissible frame temperature of C60H-DC.

Published date: 13 September 2018

The C60 HDC MCB is complied with IEC-60947 standard. 

The max operating temperature is 70°C; that mean: 
-material of operating handle => 70+25 = 95°C 
-material of case and cover => 70+50 = 120°C 
-material of external connection terminal => 70+60 = 130°C

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.