undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to SET LOGOUT TIMEOUT in ADM submenu function for AP5202 model ?
Follow the below steps :

Sets the delay time that must occur before a user is logged
off, when there is no console input for the number of minutes
specified.
To set the timeout value, type a value from 0 to 180 minutes,
and press ENTER. A value of zero (the default) disables this
function; it will display as OFF.

Schneider Electric India

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: