{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the instruction on ATV71 IBR and BRT setting.
Brake release current (IBR); Adjust the brake release current to the rated current indicated on the motor. During testing, adjust the brake release current in order to hold the load smoothly.
=> If IBR is too high, it makes some torque oscillation during the BRT time, and this oscillation can be the root cause of load slipping.
Brake release time (brt): Set according to the type of brake. It is the time required for the mechanical brake to release.


Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: