Browse FAQs

How is the memory management of LMC078 controller?

Published date: 31 March 2019

The RAM size is 512 MBytes and used for system variable(%I, %Q, %M) and also for user symbols, variables, application, and libraries.
This should be always enough for each kind of customer application and there should be no need to test it.
The NVRAM size is only 128 KBytes and used retained and/or persistent retained variables.
This means there is a limit of around 32000 persistent retained variable from datatype REAL.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.