Browse FAQs

What are the pins to apply rated 24V power supply to disable 'dIS' state of the drive.

Published date: 28 June 2019

Dis state on drive means ‘Switched On Disabled’ and it is not an error.
If not using power safety function, then apply 24V DC to PWRR_A and PWRR_B at pins 37 & 38 of CN1 to disable the state.



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.