Browse FAQs

Why Backup Set Text is Showing Red in EBO.

Published date: 29 June 2019

Kindly refer the below Backup sets color code: -

1. Black text indicates that the backup set is compatible with the current version and type of the EcoStruxure BMS server. The system highlights the selection in blue.
2. Red text indicates that the backup set is incompatible with the current version and type of the EcoStruxure BMS server. The system highlights the selection in red.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.