Browse FAQs

What does it mean if STS led of STBNIP2311 is blink 8 times

Published date: 29 June 2019

The STS LED binking 8x is related to a "TR_EVT_FATAL_ERROR" event, which could be caused by the modules inability to obtain a MAC address or to obtain configuration data. 
It means that the module is faulty and it has to be replaced.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.