Browse FAQs

what is the isolation voltage between the housing and the electronics of the XT112S1PCL2 capacitive sensor

Published date: 29 June 2019

XT112S1PCL2 capacitive sensor in plastic casing supplied in Ue=24Vdc, according to the IEC 60947-5-2 standard, rated isolation voltage is 75Vdc

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.