Browse FAQs

Do all ATV12 Drives come with EMC Filter

Published date: 29 June 2019

It's depend of ATV12 range : 
  • ATV12.....F1 and ATV12......M3 drives are designed without embedded EMC filter.
  • ATV12.....M2 have built in EMC filter. And it's possible to deactivate it with the IT jumper on the product.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.