Browse FAQs

For which application Micrologic 5 A-Z trip units are used.

Published date: 29 June 2019

Micrologic 5.2 A-Z and 5.3 A-Z are dedicated to 16 Hz 2/3 networks.They use  suitable sampling frequency. The protection settings are identical to those of Micrologic 5 A. They also offer a current-measurement function for this specific frequency.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.