Browse FAQs

Is access to micrologic of Compact NSX protected by password.

Published date: 29 June 2019

Remote access to data on Micrologic trip units is protected by password. Remote access includes:

 The communication network
 Ecoreach software
 FDM128 display

Two passwords are defined:

 the level 3 password
 the level 4 password

The level 4 password is required to write the settings to the Micrologic control unit using the Ecoreach software.

Each intrusive command via the command interface is protected by a password. The password level for each intrusive command is indicated in the description of the command.

No password is required for non-intrusive commands through the command interface.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.