Browse FAQs

Is it possible to confirgure Pre Alarms in Micrologic E

Published date: 29 June 2019

Micrologic E control units can be set to deliver pre-alarms via their optional M2C contacts. These pre-alarms can be used to warn operators that the current is approaching a trip threshold.
In this way, remedial measures (e.g. load-shedding, maintenance, etc.) can be taken before the circuit breaker trips, avoiding unnecessary shutdowns.

Two types of pre-alarms are available, depending on the control unit.
Long-time protection pre-alarm: all Micrologic E control units can be set to deliver a pre-alarm via one of their two outputs when the current reaches 90 % of the long-time protection current setting Ir.
Ground-fault protection pre-alarm: Micrologic 6.0 E control units can also be set to deliver a pre-alarm via one of their two outputs when the current reaches 90 % of the ground-fault protection pickup Ig.
Both Ir and Ig pre-alarms can be implemented if neither of the two outputs are required for other functions.

Check attached documents for an example of how to set an output to implement these or other functions

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.