Browse FAQs

Deleting an existing server in the 'IEC 61850 configurator' used for BME NOP 0300 module configuration in Unity Pro

Published date: 30 June 2019

You can delete the IEC 61850 server instance that is currently displayed in IEC 61850 Server window. To delete the server, follow these steps:

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.