Browse FAQs

Exporting the Server to an Excel Spreadsheet file from the 'IEC 61850 configurator' used for BME NOP 0300 module configuration in Unity Pro

Published date: 30 June 2019

You can export the configured IEC 61850 server that is currently displayed in IEC 61850 Server window, as an Excel 97-2003 spreadsheet file. To export a server, follow these steps:
  1. Click the Export to Excel button. Result: The Save As dialog opens.
  2. In the Save As dialog:
     Navigate to the location where you want to save the exported file.
     Click Save.
The exported Excel spreadsheet file populates the following fields with configured server data:
 Reference: the path and name of the data item
 BasicType: the data type of the item
 FC: the functional constraint value of the data item
 DO/DA: the type of item: data object (DO) or data attribute (DA)
 Initial Value: The initialized value assigned to the data item
All other fields in the spreadsheet are not populated.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.