On ATV320; Ctt is [Standard] (Std) at factory default.
Note: Brake logic control can only be assigned if [Motor control type] (Ctt) is not set to [Standard] (Std), [V/F 5pts] (UF5),[V/F Quad.] (UFq) or [Sync. mot] (SYn).
=>Assign Ctt to [SVC V] then it would be possible to program BLC to R2 on ATV320.
Note: Brake logic control can only be assigned if [Motor control type] (Ctt) is not set to [Standard] (Std), [V/F 5pts] (UF5),[V/F Quad.] (UFq) or [Sync. mot] (SYn).
=>Assign Ctt to [SVC V] then it would be possible to program BLC to R2 on ATV320.
Released for:Schneider Electric India