Browse FAQs

Does part number K1D004NX comes with rotary handle.

Published date: 30 June 2019

K1D004NX part number is stepping switches, single-pole, without “0” position “body” only.
So, the rotary handle is not included in the part number K1D004NX.
The part number of Circular heads (rotary handle) for K1D004NX is KAXZ1M12. KAXZ1M12 is Standard black handle.
And legend part number is XBCY7221.
So, the complete stepping switch with Circular heads (rotary handle) & with legend = K1D004NX+ KAX Z1M12+ XBCY7221
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.