Browse FAQs

Does Vamp 255 supports Ethernet IP & Modbus TCP communication at same time

Published date: 12 July 2019

Yes, Vamp 255 supports Ethernet IP & Modbus TCP communication at the same time. User needs to enable both the protocols in Protocol configuration.
Make sure the port number for Ethernet Ip is 44818 & port number for Modbus TCP is 502.

Use "simple tester tool" to fetch the data. You can find the tool in the below-mentioned link 
https://m.vamp.fi/documentation/ 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.