The BMXERT1604T module has16 descrete inputs that can be configured with the following 3 main functions:
Counter: This function counts pulses from the discrete input channels.
Discrete input: Standard discrete input without time stamping.
Time stamping: The discrete input with the time stamps recorded to mark input state changes.
The inputs are in 4 groups that contain 4 input channels in each group. Input functions can be configured by input group:
Input Group
Input Channels
Selectable Functions
0
0, 1, 2, and 3
Only time stamping
1
4, 5, 6, and 7
Counter
Discrete input
Time stamping (default)
2
8, 9, 10, and 11
Counter
Discrete input
Time stamping (default)
3
12, 13, 14, and 15
Counter
Discrete input
Time stamping (default)
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.