Kindly find the steps to configure output voltage for UPS SRC1KXLI
1.Press SELECT button to enter the UPS settings.
2. Navigate through the parameters using SELECT button.
3. Press ENTER/MUTE button to edit a Output voltage. The icon starts flashing to indicate it is ready for editing.
4. user selectable options are 200, 208, 220, 230 (default), 240 Vac.
5.Press ENTER/MUTE button to select the desired option, the flashing of icon stops after the selection.
Note:Output voltage can be set only when ups is in standby mode.
Released for:Schneider Electric India