Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
Limit switches XC - XCKJ80541H7 limit switch cross-reference
The complete limit switch XCKJ80541H7, discontinued, can be replaced by the 3 following sub-assemblies ZCKJ8H7 contact body + ZCKE05 head + ZCKY41 variable length thermoplastic roller lever
To get the XCKJ80541D limit switch,you just have to assemble the 3 following sub-assemblies ZCKJ8D contact body with M12 connector + ZCKE05 head + ZCKY41 variable length thermoplastic roller lever
To get the XCKJ80541D limit switch,you just have to assemble the 3 following sub-assemblies ZCKJ8D contact body with M12 connector + ZCKE05 head + ZCKY41 variable length thermoplastic roller lever
Attachment(s)
Did this answer your question?
Explore more
Explore more