How can we help you today?

How to update and build logic of Scada Pack x70 Remote Connect?

Update & Build Logic button on the SCADAPack x70 Logic page is used to build the application and update the logic variables in SCADAPack RemoteConnect with any new variables created in the SCADAPack x70 Logic Editor.
This button is available only when the SCADAPack x70 Logic Editor is open. If you have pending updates that have not been applied, or if there are any validation errors, the button is not available.

To update variables and build logic
1.On the Configuration tab, select SCADAPack x70 Logic.

1

2. If you used the SCADAPack x70 Logic Editor to modify or create your own DDT structures containing T_SPx70_xxxx variables, analyze the DDT structure definition using Build > Analyze or CTRL+SHIFT+B in the SCADAPack x70 Logic Editor before proceeding.
3. Click Update & Build Logic.
In a new project, save the project to enable the Update & Build Logic button.
You are prompted to confirm that you accept that the SCADAPack RemoteConnect configuration and logic will be modified, and that the project file will be saved.

3

4.To proceed with the operation, click Yes.
The SCADAPack x70 Logic Editor may prompt you to confirm modifications to the application. If the build operation does not complete, check whether you need to acknowledge this prompt in the SCADAPack x70 Logic Editor.

4a

In the SCADAPack x70 Logic Editor, the following message is displayed:

4b

5.To maintain synchronization of the variables in the SCADAPack x70 object database and the SCADAPack x70 Logic Editor, click Yes.
If you click No, you will be unable to build your application. A message similar to the following is displayed in SCADAPack RemoteConnect:

5

6. Click OK and then click Update & Build Logic.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings