EcoStruxure Industrial Device
EcoStruxure Industrial Device is a mobile app designed for maintenance teams monitoring, controlling and configuring IoT devices. This mobile app supports the collection, visualization, and evaluation of local device data. Changing device settings and controlling the device remotely is another feature of the mobile app, which depends from the device capabilities. Using this mobile app the diagnostic and maintenance activities gets more efficient and therefore with it saving the users time.
The core functions are:
‒ Discover: connects a device via an access point.
‒ Diagnose: visualize diagnostic data of the connected device.
‒ Configure: set and update device parameters.
‒ Update: device application download or device upgrade from the cloud.
SUPPORTED DEVICES
- PacDrive LMC Pro/Pro2/Eco
A library is needed on the device side (shipped with the app)
The core functions are:
‒ Discover: connects a device via an access point.
‒ Diagnose: visualize diagnostic data of the connected device.
‒ Configure: set and update device parameters.
‒ Update: device application download or device upgrade from the cloud.
SUPPORTED DEVICES
- PacDrive LMC Pro/Pro2/Eco
A library is needed on the device side (shipped with the app)
Close
Also available on...
| Size | iOS: 273,11 MB / Android: 45,09 MB |
| Price | Free |
| Languages | English |
Scan QR codes with your phone