Esistono delle variabili per comprendere su una cpu M580 se è in errore e quale è la motivazione ?
Le cpu M580 hanno delle system word di diagnostica per comprendere se sono in errore e quale è la causa:
Description of System Words %SW124 to %SW127
| %sw124 cpuerr %SW125 BLKERRTYPE | Function | Last fault detected | ||
| Initial State | – | |||
| Platforms | M340: Yes M580: Yes M580 Safety: Yes | Quantum: Yes Momentum: Yes | Premium: Yes Atrium: Yes | |
| The code of the last fault detected is given in this word. The following error codes cause the PLC to stop if %S78 is set to 1. %S15, %S18 and %S20 are always activated independently of %S78:
NOTE: The following codes 16#8xF4, 16#9xF4, and 16#DEF7 indicate an error on Sequence Function Chart (SFC). NOTE: The codes listed above is a non-exhaustive list. | ||||
| %SW126 ERRADDR0 %SW127 ERRADDR1 | Function | Blocking error instruction address | ||
| Initial State | 0 | |||
| Platforms | M340: Yes M580: Yes M580 Safety: Yes | Quantum: Yes Momentum: Yes | Premium: Yes Atrium: Yes | |
| NOTE: Only used for support. Address of the instruction that generated the application blocking error. For 16 bit processors, TSX P57 1••/2••:
For 32 bit processors:
For a system STOP due a watchdog overflow:
| ||||