Japan

シュナイダーエレクトリックのWebサイトへようこそ

シュナイダーエレクトリックのWebサイトへようこそ。

別の国を選択し提供している製品をご覧いただけます。また、グローバルWebサイトでは会社情報をご覧いただけます。

別の国または地域を選ぶ

  • Default Alternative Text

    効率的で人々を喜ばせるイノベーション

    会場をアイスリンクからバスケットボールのコートに1日で変えるということは、とても大胆なアイデアです。PNC Arenaは、EcoStruxure™ Buildingによってアリーナの状態を効率的に管理できるため、会場の変更を最適化し、ファンやプレーヤーに快適さを提供するとともに、その事業を発展させています。

    EcoStruxureについて
  • PNC Arena case study

    Mastering the environment for maximum comfort and efficiency

Challenge

• PNC Arena in Raleigh, NC hosts a myriad of events ranging from major concert tours to family shows on ice, all of which require unique optimal conditions.

• Switching from a basketball court to an ice hockey rink, and then to a stage show with special smoke effects, can be much easier with the right tools.

Raleigh_1147-1440x588

Solution

Efficiency and Reliability with EcoStruxure
   Apps, Analytics & Services : Resource Advisor

• Schneider Electric’s Building Management System (BMS) helps PNC Arena master its environment by allowing full control and automation of all the HVAC components: fans, motors, the air intake and outtake, humidifiers and dehumidifiers.

• BMS allows for real-time, precise monitoring of the arena, and for changes to be automated through the push of a button.

• It contributes to creating the optimal conditions that meet the requirements of the NHL or the NCAA, and helps cut down on energy costs by managing energy more wisely.

Innovation at Every Level”によって、どのようにビジネス を成功させられるかをご覧ください。

確認する

カスタマーストーリーをもっと見る

ここをクリック

プロジェクトのスナップショット

  • Default Alternative Text Energy Savings
  • Default Alternative Text Maintain Optimal Environments
  • Default Alternative Text Access Data in Real Time
  • Default Alternative Text Full Control and Automation

Results

• 770,000 square feet
• 65+ events hosted annually
• A fully controlled and automated environment.
• Not a single game cancelled due to poor playing conditions
• A $300,000 decrease in utility bills over 6 years is credited mostly to Schneider Electric’s BMS