Japan

シュナイダーエレクトリックのWebサイトへようこそ

シュナイダーエレクトリックのWebサイトへようこそ。

別の国を選択し提供している製品をご覧いただけます。また、グローバルWebサイトでは会社情報をご覧いただけます。

別の国または地域を選ぶ

  • Default Alternative Text

    1,500の生物種のための持続可能なスペース

    エネルギーの使用を減らしながらも、1,500種以上の生物の生息環境をひとつ屋根の下で調整するということは、とても大胆なアイデアです。シェッド水族館は、EcoStruxure™ Buildingを使用し、2020年までにエネルギーコストを50%削減する目標を立て、誰にとっても持続可能で快適な環境を作り出しています。

    EcoStruxureについて
  • Using technology to connect people to animals. John G. Shedd Aquarium Case Study

    Creating and maintaining environments where people connect to animals

Challenge

• Shedd Aquarium is currently home to more than 1,500 species, including fish, marine mammals, birds, snakes, amphibians, and insects from all over the world.

• In 2013, the aquarium committed to an ambitious goal of cutting energy consumption in half by 2020. Achieving that goal meant conducting extensive research and analysis to identify problem areas.

Shedd_010-900x500

Solution

Efficiency and Sustainability with EcoStruxure
   Apps, Analytics & Services : Building Analytics
   Edge Control: BMS, SmartStruxure
   Connected Products: SVFT Drives, Turnkey Solar Solution (256kW of solar panels)

• The Schneider Electric Building Management System (BMS) allows Shedd Aquarium to manage everything inside the building from lighting, via life support systems, to HVAC.

• Through detailed mapping of the BMS, Building Analytics evaluates all equipment that’s under the BMS’s control, looks for faults in process, maintenance, and repair, and then prioritizes those based on an energy savings value.

• Variable Frequency Drives (VFDs) are used for water, HVAC, as well as for life support systems to control loads.

• Last but not least, a turnkey solar solution with 265KW of solar panels installed on the roof of the Oceanarium generates clean, renewable energy, and reduces energy costs.

Innovation at Every Level”によって、どのようにビジネス を成功させられるかをご覧ください。

確認する

Discover our Building Analytics solution.

Learn more

カスタマーストーリーをもっと見る

ここをクリック

Results

• Energy cost avoidance and road map
• More than 480,000 square feet of building
• Energy cost avoidance and road map
• Fine-tuning systems and equipment to save energy
• Fault detection and diagnostics
• Meaningful analytics and prioritized actions associated with measurable ROI
Default Alternative Text

“So what we’re doing with it is we’re essentially keeping people, animals and staff comfortable.” Bob Wengel, Vice President of Facilities, Shedd Aquarium.