Issue
Network Management Card - Single Phase Symmetra SNMP Trap #77 details
Product Line
- UPS Network Management Card 1 - AP9617, AP9618, AP9619
- UPS Network Management Card 2 - AP9630/AP9630CH, AP9631/AP9631CH
Environment
- All serial numbers
- All firmware versions
- SNMPv1 or v3 traps
Cause
SNMP trap # 77 (abnormalCondition) is reserved for specific UPS failures. When trap #77 is sent, it also has a binded subtrap which gives further detail into the nature of the fault. The subtraps are specific to the UPS family type.
Resolution
Attached is a breakdown for the Symmetra single phase line of UPS (Symmetra RM, Symmetra LX, Symmetra Power Array), which uses the Network Management Card APP called 'sy'.
게시 대상:슈나이더 일렉트릭 Korea