Issue:
A customer needs to know if all NetShelter cabinets ship with the same key.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Having a single key allows ease and simplicity for customers who own multiple cabinets. Or, someone may want unique keys on some cabinets.
Resolution:
Yes, all NetShelter SX cabinets ship with the same key for the front door, rear doors and side panels.The standard NetShelter SX replacement key is part number W870-8135.
If you would like information on unique locks for NetShelter SX cabinets please see Knowledge Base document FA158606.http://www.apc.com/us/en/faqs/FA158606/
If you need replacement keys for a NetShelter cabinet other than the NetShelter SX please see Knowledge Base document FA158623: http://www.apc.com/us/en/faqs/FA158623/
게시 대상:슈나이더 일렉트릭 Korea