How to check PME web application's CPU and Memory usage using IIS
Issue
The memory usage of web application components is needed to troubleshoot high memory use or to optimize performance
Product Line
Power Monitoring Expert 2024
Power Monitoring Expert 2023
Power Monitoring Expert 2022
Power Monitoring Expert 2021
Power Monitoring Expert 9.x
Power Monitoring Expert 8.x
Power Monitoring Expert 7.2.x
Environment
Power Management Operations
Cause
Customer would like to investigate the current usage of the PME web applications
Resolution
Internet Information Services (IIS) Manager contains a feature called Worker Processes that can be used to monitor the memory and CPU usage on the server.
1- Make sure that PME's Web Applications is already open in any supported browser.
2- Open IIS manager. That can be done by running "inetmgr" command or by searching "IIS" in the search bar. (It is recommended to run as an admin.)
3- Click on the server name.
4- Double-click on Worker Processes as shown in the picture below.
5- The worker processes will list all the Application pools in use.
Private Memory (Committed bytes) corresponds to actual RAM usage