Issue
The error "proworxaddrused.frm" gets returned when trying to open a project
Product Line
All versions of Proworx 32
Environment
Windows 7, Windows 10
Resolution
This error will get returned if you updated to a patch immediately after installing 'ProWORX 32' without
rebooting the PC.
To resolve the problem,
- Insert the installation CD and start the install process.
- Select the repair option to perform a repair.
- Reboot the PC.
- Apply the patch update.
Опубликовано для: Schneider Electric Казахстан